Why my wio terminal display becomes black if i program it with circuit python and runs fine in arduino firmware

screen becoming black after uploading circuit python code even after having correct libraries

probably something with the display/graphics library

Hi there,

and welcome here…

So which Board Support Package are you using and which Display LIB, specifically?
are you following a guide or WiKi example. you’ll need to provide more info to get better answers. Post up the code using the code tags above" </>" paste it in there… 123, ABC
Bob is your uncle.

HTH
GL :slight_smile: PJ :v:

now displays are working good but will circuit python support wifi and bluetooth on wio terminal
thank you,
Preamnath