Where is XIAO-ESP32S3-KWS_inferencing.h?

Help me! Where I can find the file?

D:\adruino\project\XIAO-ESP32S3-Sense\XIAO-ESP32S3-Sense-main\xiao_esp32s3_microphone\xiao_esp32s3_microphone.ino:46:10: fatal error: XIAO-ESP32S3-KWS_inferencing.h: No such file or directory
46 | #include <XIAO-ESP32S3-KWS_inferencing.h>
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
exit status 1

Compilation error: XIAO-ESP32S3-KWS_inferencing.h: No such file or directory

I had the same question so did a search. The XIAO-ESP32S3-KWS_inferencing.h is created when the model and example programs are downloaded from the Edge Impulse site when the project is called XIAO-ESP32S3-KWS-inferencing.
However, I found it in the zip file at the github site:

You’ll need to d/l the zip file and unzip it. Then look under the directory for:
TinyML-main\XIAO-esp32-S3-Sense\KeyWordSpotting(KWS)\src