In lieu of circuitpython reference, I installed ardupy. It works but the aip tool is giving errors. Is it my python 3.8.3 version?
Traceback (most recent call last):
File “c:\program files (x86)\python38-32\lib\runpy.py”, line 194, in _run_module_as_main
return _run_code(code, main_globals, None,
File “c:\program files (x86)\python38-32\lib\runpy.py”, line 87, in run_code
exec(code, run_globals)
File "C:\Program Files (x86)\Python38-32\Scripts\aip.exe_main.py", line 7, in
File “c:\program files (x86)\python38-32\lib\site-packages\aip\main.py”, line 52, in main
from aip.command import commands_dict, parse_command
File “c:\program files (x86)\python38-32\lib\site-packages\aip\command.py”, line 46, in
from aip.build import buildCommand
File “c:\program files (x86)\python38-32\lib\site-packages\aip\build.py”, line 34, in
from pip._internal.operations.prepare import (
ImportError: cannot import name ‘_download_http_url’ from ‘pip._internal.operations.prepare’ (c:\program files (x86)\python38-32\lib\site-packages\pip_internal\operations\prepare.py)
The iap.exe seems to run OK. It returns board info as 2020-08-14.