What is the smallest 3.7 VDC LIPO Battery for an ESP32C3 with continuous BLE?

BenderBud,
Please give me information for my study.

  1. Is the module you are using the same module as the picture I showed?
  2. If so, what kind of charger (how many watts) is connected to the modue?

Please use this as a reference for your project.
I measured the current consumption with the sketch in the link below and it was average 80mA and peak 150mA. 150mAh or 500mAh battery might be too small.

1 Like