Greetings,
For this EMG sensor: https://wiki.seeedstudio.com/Grove-EMG_Detector/
I believe one electrode is a reference (that can be placed farther away on the skin) and one is placed near the end of a muscle, and one near the middle of the same muscle. However, I’m not sure which color is which. If I want to experiment with monitoring another muscle besides the arm, what is general rule for where where the red, white and black electrodes should be placed for a given muscle?
Also, can the reference electrode be placed much farther away from the particular muscle, does it need to be within a certain number of inches on the same arm or leg, for instance – could the reference electrode be placed on the right arm, if the other two electrodes are on the left arm, for instance?
Thanks for any guidance!