Welcome to the RePhone Community!

Hello out there,
I have a similar problem, The original battery was dead, (as the kit was unused for 3 years)
I connected a single cell charged to 4,1V to the board.
The board begun to reboot constantly.
Now as the battery is lower on voltage, the situation seems to be stable.
Is there any upper limitation on the input voltage?