obama
August 17, 2020, 1:09pm
1
I have a problem:
I am using the sample grove_water_sensor.py
it constantly prints “255” until it touches water or my finger, then it just freezes and does not output anymore.
When i “Ctrl + C” it after it froze, it show this error message:
^CTraceback (most recent call last):
File “grove_water_sensor.py”, line 50, in *
print(grovepi.digitalRead(water_sensor))*
File “/home/pi/Dexter/GrovePi/Software/Python/grovepi.py”, line 249, in digitalRead*
data = read_identified_i2c_block( dRead_cmd, no_bytes = 1)[0]*
File “/home/pi/Dexter/GrovePi/Software/Python/grovepi.py”, line 242, in read_identified_i2c_block*
data = read_i2c_block(no_bytes + 1)*
File “/home/pi/Dexter/GrovePi/Software/Python/grovepi.py”, line 232, in read_i2c_block*
raise KeyboardInterrupt*
KeyboardInterrupt
since i am not really good in python, i could use a little help, thanks already for any answers
I already reinstalled and checked the “Dexter” installation, i even reinstalled the whole raspberry OS new.
(also my English isn’t quite top notch, sorry)
Baozhu
August 18, 2020, 12:56am
2
Is your hardware connected? Could you please provide a picture of the connection of the hardware?
obama
August 18, 2020, 6:37am
3
Sure, here you go:
As you can see in the picture, i also have an RGB-LCD attached, which works perfectly fine.
Also earlier, i had the sensor attached on an RPI with an Base hat and there it worked just fine.
Thanks in advance
Baozhu
August 20, 2020, 12:07am
4
Will it work if it is not connected to RGB-LCD?It could be an incompatibility problem between devices.
obama
August 24, 2020, 12:00pm
5
Hi. Thanks for the reply.
Nope, its exactly the same error if i run it without the lcd connected.
I also tried using all the “D” Ports, but its the same error for every single one.
Baozhu
August 26, 2020, 12:22am
6
There must be some problems here.Grove-Water_Sensor is a simple IO device.But the i2C error appears in your error. Please check our Wiki documentation.
https://wiki.seeedstudio.com/Grove-Water_Sensor/#play-with-raspberry-piwith-grovepi_plus
obama
August 31, 2020, 9:33am
7
I read the Wiki and once again followed the Installation there step by step.
Still the exact same Error
Is it pssible, that it could be bacause of the Raspberry? Its an RPI2 Model B.
Also. On the base hat, the sensor works. I know its a stupid idea, i just ask to be absolutely sure that this is not a solution: Could i stack the Base hat and the GrovePi+ on top of each other and connect the RGB LCD on the GrovePi+ and the Water Sensor on the Base hat?
Again, thanks in advance