Actually, I just tried it. My code seems to work, but at some point it showed “Remote I/O error” (I’m not sure if I might have induced the error by accidentally touching the wires on the breadboard, though)
I had to compile the micropython library on my Pi: https://www.raspberrypi.org/forums/viewtopic.php?t=191744
Please see the code and the screenshots:
import time
import smbus
import numpy as np
NO_TOUCH = 0xFE
THRESHOLD = 100
ATTINY1_HIGH_ADDR = 0x78
ATTINY2_LOW_ADDR = 0x77
i2c_ch = 1
i2c_address1 = 0x77
i2c_address2 = 0x78
# Register addresses -- don't know what they are for
reg_temp = 0x00
reg_config = 0x01 # offset?
bus = smbus.SMBus(i2c_ch)
def getHigh12SectionValue():
high_data = bus.read_i2c_block_data(ATTINY1_HIGH_ADDR, reg_config, 12)
return high_data
def getLow8SectionValue():
low_data = bus.read_i2c_block_data(ATTINY2_LOW_ADDR, reg_config, 8)
return low_data
def check_water_level():
sensorvalue_min = int(250)
sensorvalue_max = int(255)
low_count = int(0)
high_count = int(0)
touch_val = int(0)
trig_section = int(0)
low_count = 0
high_count = 0
low_data = getLow8SectionValue()
high_data = getHigh12SectionValue()
for i in range(8):
if low_data[i] > THRESHOLD:
touch_val += 1
for i in range(12):
if high_data[i] > THRESHOLD:
touch_val += 1
value = touch_val * 5
print("water level = " + str(value) + "%")
while True:
check_water_level()
time.sleep(2)
Here’s a short video on how my code works:
Here’s the error message I got in the end, but now the code runs for a few minutes and nothing happens - so it probably was by accident:
I believe my code lacks some sensor diagnostics, e.g. if the bus actually could be read, or - I’m not using the NO_TOUCH variable, which probably determines some sensor parameters or readouts. I did not figure out how to use it from the Arduino code. If you would have any ideas on how to improve this, please share ![]()