I am trying to use the “Grove Water Level Sensor” with an ESP8266 (and tried ESP32) and ESPHome and this doesn’t seem to work. I have connected the SDA/SDL to D1/D2 (used no resistors and 4k7 ones) on my ESP8266 and the code detects the address “0x77” during the I2C scan. This means the sensor is detected.
What level of water i try, i always get 0% or 5% in my output. For 30-35% i see the following bytes read:
[09:51:10][V][custom:033]: low 8 sections value = 222.0.0.0.0.0.249.0
[09:51:10][V][custom:035]: high 12 sections value = 249.249.249.249.249.248.0.0.0.0.0.0
[09:51:10][V][custom:049]: touch_val = 16193
[09:51:10][V][custom:057]: water level = 5
I use the following code in ESPHome (mostly copy-paste from the example):
#include "esphome.h"
// https://wiki.seeedstudio.com/Grove-Water-Level-Sensor/
unsigned char low_data[8] = {0};
unsigned char high_data[12] = {0};
int sensorvalue_min = 250;
int sensorvalue_max = 255;
#define NO_TOUCH 0xFE
#define THRESHOLD 100
#define ATTINY1_HIGH_ADDR 0x78
#define ATTINY2_LOW_ADDR 0x77
class WaterLevelSensor : public PollingComponent, public Sensor {
public:
WaterLevelSensor() : PollingComponent(15000) {}
void setup() override {
// Initialize the device here. Usually Wire.begin() will be called in here,
// though that call is unnecessary if you have an 'i2c:' entry in your config
ESP_LOGV("custom", "in-setup");
Wire.begin();
}
void update() override {
uint32_t touch_val = 0;
uint8_t trig_section = 0;
getLow8SectionValue();
getHigh12SectionValue();
ESP_LOGV("custom", "low 8 sections value = %d.%d.%d.%d.%d.%d.%d.%d", low_data[0], low_data[1], low_data[2], low_data[3], low_dat a[4], low_data[5], low_data[6], low_data[7]);
ESP_LOGV("custom", "high 12 sections value = %d.%d.%d.%d.%d.%d.%d.%d.%d.%d.%d.%d", high_data[0], high_data[1], high_data[2], hig h_data[3], high_data[4], high_data[5], high_data[6], high_data[7], high_data[8], high_data[9], high_data[10], high_data[11]);
for (int i = 0 ; i < 8; i++) {
if (low_data[i] > THRESHOLD) {
touch_val |= 1 << i;
}
}
for (int i = 0 ; i < 12; i++) {
if (high_data[i] > THRESHOLD) {
touch_val |= (uint32_t)1 << (8 + i);
}
}
ESP_LOGV("custom", "touch_val = %d", touch_val);
while (touch_val & 0x01)
{
trig_section++;
touch_val >>= 1;
}
ESP_LOGV("custom", "water level = %d", trig_section * 5);
publish_state(trig_section * 5);
}
void getLow8SectionValue(void)
{
memset(low_data, 0, sizeof(low_data));
Wire.requestFrom(ATTINY2_LOW_ADDR, 8);
while (8 != Wire.available());
for (int i = 0; i < 8 ; i++) {
low_data[i] = Wire.read(); // receive a byte as character
}
delay(10);
}
void getHigh12SectionValue(void)
{
memset(high_data, 0, sizeof(high_data));
Wire.requestFrom(ATTINY1_HIGH_ADDR, 12);
while (12 != Wire.available());
for (int i = 0; i < 12; i++) {
high_data[i] = Wire.read();
}
delay(10);
}
};
It is a pity, the Grove sensor had huge potential.