Wake on Bluetooth Connect (alternatively, power consumption)

Hi there,

So bottom line is Both CAN’t be true,…
“Sleep” or “Listening for BLE packet” BLE is not magic. It’s just a radio.

For a device to “hear” a BLE packet, three things must be ON:

  • RF front end (radio hardware)
  • Clock system (timing is everything in BLE)
  • BLE stack / controller

When you put an ESP32 (or most MCUs) into deep sleep, all of that is completely powered down.

:backhand_index_pointing_right: No radio
:backhand_index_pointing_right: No receiver
:backhand_index_pointing_right: No packet detection
:backhand_index_pointing_right: No chance of waking from BLE

Deep sleep exists for one reason:

Ultra-low power (µA range)

Keeping the radio on—even in a “listening” mode—costs orders of magnitude more power.

Typical comparison:

Mode Current Draw
Deep Sleep ~5–20 µA
BLE idle/listen ~1–10 mA

That’s a 100x–1000x difference.

So if BLE wake were allowed in deep sleep, it wouldn’t really be “deep sleep” anymore.
Some chips (not ESP32) have special ultra-low-power radios or “wake-on-radio” features—but even those:

  • don’t run full BLE stacks
  • use simplified detection
  • still consume more power than true deep sleep

I have this diagram I made for the (10) BLE sensor_Node project with 3 concurrent connections and 6 notifies. (demo & code is one here)

I useds the technique # 4 along with the #2 the timer.

https://forum.seeedstudio.com/t/multi-concurrent-ble-connections-with-seeed-round-display/293997

HTH
GL :slight_smile: PJ :v: