Hi, I just bought a W5500 Ethernet shield, trying to figure out how to configure the SPI pins to work with the mbed OS W5500 driver. I downloaded the above schematic, but it doesn’t show the Arduino connectors JP1,2,4 or 5 (or JP3 for that matter). Nor does it identify the large IC on the first of the two pages marked Sheet 1 of 1. Thanks
Hi @jmporter34, Which connectors are you looking for? also you can find the Ethernet Shield V1.0 Eagle Files from here and detailed information from the W5500 Ethernet Shield Wiki Page here