W5200 Ethernet Shield BUG?

The problem is R3 is not to ground connected and the logic state of the pin 45 is casual is not low or high.
From the W5200 datasheet:

In the eagle files if you drag R3 and move it you can see is connected only to the site of pin 45 and not in the other site to ground.
Maybe if you connect the r3 to ground and reconnect the cutting connection work good.