W5200 Ethernet Shield BUG?

I still have trouble getting the shield to work. When I use the examples of the library the Webserver example works, but the webserver with SD card is not working, Via serial i see it is able to read and write from the SD card, but the IP adress is not correct, it becomes 255.255.255.255. Any one has the same problem with the example?