I have a Arduino-Mega and the tft seeedstudio 2.8.
And the library for Arduino
I try to make a volt-amp meter 0-300v 100ma
All is working wel, only the display gives a question mark by reading the output off a sensorValue.
This is an example.
Can you give me an example.
This is my first project with Arduino
With a GLCD Screen is not a problem.
But with a TFT is different.
Thanks in advance.
Piet
In line 4 you convert a float (4 byte arduino.cc/en/Reference/Char).
If voltage_string (better variable names?) is larger then 127 your result is wrong.
Tft.drawChar routine is for print a single ASCII char. Not for Numbers.
You must write a routine (if there is no in the tft library) to show float numbers. (arduino.cc/playground/Main/FloatToString)
If you don’t know to handle this please read: google.com
Don’t know if this helps or not, but I wanted to display int values and took this approach. I force the screen to redraw the original text to update what was there (assuming black background). Of course this is for integer values not float.
intTextUpdate(oldx,newx,80,20,2,BLUE);
void intTextUpdate(int origVal, int newVal, int xpos, int ypos,int fsize, int fcolor){
String fcColor;
intTextDisplay(origVal,xpos,ypos,fsize,BLACK);
intTextDisplay(newVal ,xpos,ypos,fsize,fcolor);
}
void intTextDisplay(int dispval, int xpos, int ypos, int fsize,int fcolor)
{
char iTocVal[6];
String(dispval).toCharArray(iTocVal,6);
Tft.drawString(iTocVal,xpos,ypos,fsize,fcolor);
}