First of all, this application has become very useful, job well done. After extensive use of v1.0.0.4, I have some suggestions.
- With the trigger index button, single click as it is now, double click to center the trigger on the screen. Same with the Max Min buttons.
- Voltage offset, can you set the voltage offset to zero with a double click on the slider button or provide a separate button?
- Sample offset and Time Index are confusing me. Should they both be called Trigger Offset? The Nano references everything to the Trigger.
- The current waveform area could be called the Viewing Window with it’s current tabs. The current XML profile area could be called the Data Window with it’s own tabs. One tab could be XML Profile Data and another tab could be Cursor Data, with room for more additional tabs later as required.
- Add voltage cursors similar to the time cursors and place all that data results under the new Data Window’s Cursor Data tab.
- It appears that you are preparing for multiple scope inputs under the Configuration Tab?
- I will create a data train xml file tomorrow to test the logic analyzer portion. I will include data stream parameters and make it available in this thread.
- Instead of writing a users guide, I would be glad to make a user video series if you like. It has been proven that when a programmer (You) sees another’s interpretation of how the program works (Me), it provides new insight to the programmer, and usually results in improvements.
- The program name “XML Data Viewer” could be more generic and would stand on its own irregardless of the XML file creator such as DSO Nano or DSO Quad (MiniDSO) or some other application as yet unknown.
These are all suggestions which I believe you are asking for. I am very impressed with the functionality that has been gained thus far. It will completely eliminate my use of Excel for viewing XML files. I expended a good amount of effort learning Excel XML, but will gladly throw it all away for this!