Had my Nano for a week and have been studying the posts on this board.
I have question about versions:
When turned on, startup screen reads
[size=150]Nano v. 1.1 (at top)
firmware version 2.02 (at bottom)[/size]
Circuit board edge near battery reads
[size=150]DSO201V1.3A[/size]
What versions do I have? I am confused trying to decide what comments apply to my device.
I purchased my Nano from NKC Electronics in the US two weeks ago.
Thank you very much for any help
Nano v. 1.1 (at top) : The DSO Nano version (model)
firmware version 2.02 (at bottom) : the firmware version
DSO201V1.3A : the hardware version
Thanks. Now I think I know where I am.
So far, I think I have
file reading/saving with SD disk working
DSO recognized by 3 Dfuse software programs
Next steps are to try upgrading firmware.
Also, not sure about best procedure for charging battery - in device or remove and use separate Li Bat charger?
The safest way is the charge circuit of cause, but it also has some issues .the circuit now is also acceptable and really work in most simplicity MP3,MP4 machine.
FreeZinG:
Nano v. 1.1 (at top) : The DSO Nano version (model)
firmware version 2.02 (at bottom) : the firmware version
DSO201V1.3A : the hardware version
sorry, but i don’t understand…whic difference between
The DSO Nano version (model)
and
firmware version 2.02 (at bottom) : the firmware version
in my unit (an e-design unit, but don’t worry, i know you after i’ve buied the unit! )
at startup i’ve only
version 1.5.20P ( i think paul version 1.5.20), is then all ok?
for knowing the hardware version i must open the back panel?
ESP
July 14, 2010, 1:29pm
6
You could try different firmware on any version whenever needed.
Check it out here: code.google.com/p/dsonano/