Hi,
I’m trying to use the UART on a XIAO nrf52840 in MicroPython but I’m not getting any response.
So I’d like to troubleshoot the UART.
Say I use the most basic code:
from machine import UART
modem = UART(0, 115200)
modem.init()
How can I now check the defaults for bits/parity/stop/rx/tx ?
Also, is UART 0 reserved for the REPL? I’m using Thonny and I’m printing on USB, does that mean I can’t use UART 0?
Thanks!
Hi there.
So not being a Python guy, I do see this working, YMMV
import serial
ser = serial.Serial(
port = '/dev/ttyUSB0',
baudrate = 115200,
timeout = 10,
xonxoff = False
)
ser.reset_output_buffer()
ser.reset_input_buffer()
val = 0
command = ''
command = input("Enter command: ")
val = ser.write(command.encode(encoding = 'ascii', errors = 'strict'))
print("Waiting bytes: ", ser.in_waiting)
print("Bytes written: ", val)
in_data = ''
in_data = ser.read_until(b'}')
print(in_data)
HTH
GL
PJ 
Yah, thanks for your reply but it’s micropython, not python.
This topic can be closed, sorry
How did you bootload micropy i try and cant get it done?