I want to use RoundDisplay and L76K GNSS at the same time, but when I connect both, the green light on the GNSS module is always on and I can’t get the time or position. I can get the time and position just fine with the GNSS module alone. How can I use both?
How can I start using it?
Hi there,
Re-map the pins you use for reset but that’s just the beginning, the Touchscreen TPint (D7) which is the Serial port f(RX)for the uart mode of the GNSS so that’s a NO-GO as well. and the SD-card CS is also SPI
here is the Xiao FP for the Round Display.
You would need to remap the SPI (MOSI) pin just for a one on one, the Round Display adds too much complexity over an I2C display and a Xiao MCU.
HTH
GL
PJ ![]()
maybe just use another XIAO and communicate with it via bluetooth or something
Hi. I’m trying to connect this L76k module to a Raspberry Pi. Am I correct that I have to feed 5v to the WAKEUP and RESET pins as well? Right now, I only connect RX, TX, 5V, and GND to the RPi, and it does nothing.
Hi there
Yes, the wakeup pin and reset need a logic 1 or 5V pullup.
have a look at the wiki, here:
shows what is needed.
HTH
GL
PJ ![]()