So I have an arduino connected to 2 V1.3 motor drivers and I do not understand how to control them individually. If I attempt to move MOTOR1 on one driver the other drivers MOTOR1 also moves.
[code]
#define RearDriver 0x0f
#define FrontDriver 0x0a
#define FDriver Motor
#define RDriver Motor
void setup() {
Serial.begin(9600);
FDriver.begin(FrontDriver);
RDriver.begin(RearDriver);
}
void loop() {
FDriver.speed(MOTOR1, 50);
FDriver.speed(MOTOR2, 0);
RDriver.speed(MOTOR1, 0);
RDriver.speed(MOTOR2, 50);
}
[/code]
Both jumpers are connected, and the drivers are being powered via a 7.4V Lipo