Using GROVE LoRa Radio 433 or 868 MHz transmitter/recievers

Looking at these boards, but unsure about the legal side of using this frequency range in Europe? Specifically in Switzerland?

Did anybody look this sort of thing up?

the devices are very specific designed to stay in the legal framework… it has options to check for your region… obviously if you use the wrong region… it would try to transmit incorrectly

Generally in the EU 868 is primarily used and is within the legal band widths. 433 is more used for low level things like remote control devices, home automation, garage and gate remote opening etc
The 915mhz bands are for Asian (Korea, china, Japan) and American markets, although it sounds like they are going to be out of luck soon as the American airwave people have sold the frequency apparently.
Hope this helps
Alan

1 Like

Am having trouble communicating with two modules(Grove-LoRa Radio 433MHz), and I am using arduino uno cards , the codes used are complying but how to communicate with the two modules(I can’t send anything from one to another). Kindly help please anyone?

helloooo anyone???

What are you trying to do? I dont know if i would waste my time on this product as it is pretty old and the LoRa has moved so much more forward with meshtastic… with that being said, we can help you but you gotta put a little more work into it

Thank you for your response @cgwaltney . I had to contact the technical support directly for assistance as it’s an old module and I was able to communicate with the two of modules. The tip is to use the seeedstudio library directly not the Radio Head or the LoRa. Thank you again for your response and time really appreciate it.

1 Like