Hi. The WiKi says to re-flash the RTL8720 in order to use the new WIO terminal WiFi libraries.
The executable /ambd_flash_tool/tool/linux/amebad_image_tool is a 64 bit ELF. Does that mean that it’s not possible to program up the terminal if you are developing on a Raspberry Pi, or has someone ported the code somewhere?
Hi @susan091059,
Unfortunately, this tool can only run in X86 Linux systems, but not in ARM systems such as Raspberry Pi.
It works well with PC, Mac, and X86 Linux
Best Regards,
Lakshantha