I’m using an Arduino Due to read from the seeed Multichanel Gassensor. But when I upload the code “ReadSensorValue_Grove” from https://wiki.seeedstudio.com/Grove-Multichannel_Gas_Sensor/#platforms-supported , I get the error “architecture not matched”. How can I use the sensor with the Due?
We didn’t test the Arduino DUO.There may be some incompatibilities.
The Arduino Due has even 2 I2C connections, why should it not be compatible?
The sensor is part of my bachelor thesis, so it would be nice if you could help us find a solution here.
I’m really sorry that I didn’t answer your question correctly.The product you mentioned is currently being upgraded to this, the old product, which we did not test on DUO.The old product life cycle is coming to an end.
https://wiki.seeedstudio.com/Grove-Multichannel-Gas-Sensor-V2/