Hello,
I’ve recently acquired a BeagleBone Green with AM335x processor. I connect a high-speed USB device (actually a 3D camera) to the USB host port, and it recognizes well (looking at dmesg output).
When I try to read data from the camera I have a timeout and get no data ever. The ‘dmesg’ output show the errors:
musb_host_rx 1983: Rx interrupt with no errors or packet!
musb_ep_program 941: broken !rx_reinit, ep2 csr 0003
Other users seemed to have this problem in the past, and it seems related to the musb_hdrc driver itself, but I’ve not been able to find a solution and need help urgently to solve this issue.
The system version in my BeagleBoneGreen is:
Linux 4.4.9-ti-r25 #1 SMP Thu May 5 23:08:13 UTC 2016 armv7l GNU/Linux
Thanks
Ways to fix USB Device Not Recognized Error
- Restart Your Computer.
- Update Computer.
- Change USB Root Hub Settings.
- Update USB Driver.
- Check And Change Ports.
- Change USB Selective Suspended Settings.
- Format Your Drive.
Regards,
Rachel Gomez