Upgrade DSO201 Nano Firmware V3.21A

This is what I find on the internet:

[code]Bit when I hold the down (-) button and turn it on it says:
“Serial:######## License:##########
Device Firmware Upgrade V3.21A
Please copy the Hex or Bin file to the DFU virtual USB disk”

Hmm, that’s really weird. I’ve never had that happen.

It goes to the firmware install mode. I just cant get the PC to stop thinking it is a hard drive. It wont accept the Dfuse driver.

You shouldn’t need an sd card.
also, did the dso nano go into the firmware install mode or just boot normally?

I also tried manually launching the Wizard through the Device Manager and navigating to the C:\Program Files\STMicroelectronics\Softw­are\DfuSe\Driver folder but it says “The specified location does not contain information about your hardware”
I Have the DSO201 and it does not have an SD card. DO I need that to install firmware?

Hey! I need help and I can seem to find any with google.
I can’t get my DSO to show up in Dfuse as device in the popup menu.
After I install Dfuse and then turn on my DSO while holding down the button to go into firmware mode, The DSO just shows up as a drive. I never get the New Hardware wizard.
I have tried 3 different PC’s. Any ideas?
[/code]

This is exactly what hapens with my DSO201. It seems “they” have changed the upgrade process … but how???