Hello World !
I am new on this forum and for my first message, I will explain a little problem on which I work for 2 days now…
So, first, you need to know that I have a ds203 (quad) with hw2.7B and windows 10 (omg !!
)
2 days ago, I managed to update my dso but how amazed I was when I saw that my windows can’t recognize the dfu of my quad. After some readings on the net, I understood that the dfu version was the problem and so planned to update it with a newer one (3.45C).
Thus, I used a usb to ttl converter of a xbee adaptator and do the update with the 3.45C dfu. I restarted the dso and… holl** cr**, the hardware had changed on the splash screen, showing 2.81 with FPGA error. I thought it was the FPGA but quickly, I saw that it was impossible to fix it unless I downgrade the dfu to the ancient one (incompatible with w10 or 8 or 8.1 even 7)
Therefor I have two questions (actually 2,5 questions):
- Is there a way to implement the dfu 3.45 without affecting the fpga and the reste (hw showed version for instance) ?
-If no, can I even though update the system (is B164 compatible ?) and install new app (wildcat and/or gabonator) ?
Thank You in advance
Danny