I am on a Mac.
I do not see /dev/cu.usbmodem401301 as I did earlier - before flash.
This was flash error:
wio-terminal aip list
Package Version Location
------------------------------ ------- ------------------------------------------------------------------
seeed-ardupy-ultrasonic-sensor 1.0.0 https://github.com/Seeed-Studio/seeed-ardupy-ultrasonic-sensor.git /7.1s
➜ wio-terminal aip build
QSTR updated
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/foantcyemod_ardupy_ultrasonic_sensor.c.o -c /Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/mod_ardupy_ultrasonic_sensor.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-g++ -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu++11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -fno-rtti -fno-exceptions -fno-threadsafe-statics -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -std=gnu99 -U_FORTIFY_SOURCE -Os -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/oxtbkgdqwrapper_ultrasonic_sensor_hal.cpp.o -c /Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/wrapper_ultrasonic_sensor_hal.cpp
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-g++ -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu++11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -fno-rtti -fno-exceptions -fno-threadsafe-statics -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -std=gnu99 -U_FORTIFY_SOURCE -Os -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/fsjowbnuUltrasonic.cpp.o -c /Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor/Ultrasonic.cpp
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/leduwjsmobjmodule.c.o -c /Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/py/objmodule.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/fxqrvjwuparse.c.o -c /Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/py/parse.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/hqaefmntqstr.c.o -c /Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/py/qstr.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/wahfyevd__init__.c.o -c /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/__init__.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc -L/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Lib/GCC -Os -Wl,--gc-sections -save-temps -T /Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal/flash_with_bootloader.ld -Wl,-Map,/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/firmware.map -Wl,--whole-archive /Users/golden/.config/aip/ardupycore/ArduPy/lib/libmicropython.a -Wl,--no-whole-archive /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/foantcyemod_ardupy_ultrasonic_sensor.c.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/oxtbkgdqwrapper_ultrasonic_sensor_hal.cpp.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/fsjowbnuUltrasonic.cpp.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/leduwjsmobjmodule.c.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/fxqrvjwuparse.c.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/hqaefmntqstr.c.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/wahfyevd__init__.c.o -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/Ardupy --specs=nano.specs --specs=nosys.specs -mcpu=cortex-m4 -mthumb -Wl,--cref -Wl,--check-sections -Wl,--gc-sections -Wl,--unresolved-symbols=report-all -Wl,--warn-common -Wl,--warn-section-align -Wl,--start-group -lm /Users/golden/.config/aip/ardupycore/ArduPy/lib/libarm_cortexM4lf_math.a -mfloat-abi=hard -mfpu=fpv4-sp-d16 -Wl,--end-group
/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/Ardupy :
section size addr
.text 290392 16384
.ramfunc 32 306776
.ARM.exidx 8 306808
.data 432 536870912
.hsram 1024 536871344
.bss 191056 536872368
.ARM.attributes 48 0
.comment 240 0
.debug_info 1600486 0
.debug_abbrev 138683 0
.debug_aranges 21520 0
.debug_ranges 30008 0
.debug_line 212713 0
.debug_str 163071 0
.debug_frame 70816 0
.debug_loc 309661 0
.stab 204 0
.stabstr 441 0
Total 3030835
Firmware path: /Users/golden/.config/aip/deploy/Ardupy.bin
Usage:
aip flash /9.5s
➜ wio-terminal aip flash
Using cached http://files.seeedstudio.com/arduino/tools/x86_64-apple-darwin/bossac-1.8-48-gb176eee-i386-apple-darwin16.1.0.tar.gz (39 kB)
ERROR: Exception:
Traceback (most recent call last):
File "/usr/local/lib/python3.7/site-packages/pip/_internal/cli/base_command.py", line 188, in _main
status = self.run(options, args)
File "/usr/local/lib/python3.7/site-packages/aip/flash.py", line 142, in run
stty = self.stty
File "/usr/local/lib/python3.7/site-packages/aip/flash.py", line 97, in stty
return "stty -f " + self.port + " %d"
TypeError: can only concatenate str (not "NoneType") to str /1.1s
➜ wio-terminal aip board
ERROR: Sorry, the device you should have is not plugged in. /0.5s
Since then, it no longer connect via USB.