Hi,
I’m trying to upgrade my DSO Nano to BenF’s firmware for hours now.
It doesn’t work on windows and it doesn’t work on a Mac.
I only get this:
[code]dfu-util --dfuse default -a 0 -D “DSO BenF APP v3.64.dfu”
dfu-util - © 2005-2008 by Weston Schmidt, Harald Welte and OpenMoko Inc.
© 2010 Tormod Volden (experimental DfuSe support)
This program is Free Software and has ABSOLUTELY NO WARRANTY
dfu-util does currently only support DFU version 1.0
No DFU capable USB device found[/code]
Why can’t it find my device? Is it impossible to upgrade my DSO?
I have one from the beta phase, “DSO201V1.1” is written on the PCB…
Anything I can try? dfu-util --list doesn’t show anything when the DSO is connected.
When I’m connecting it with a Micro SD inserted, it appears in the devices list…
I have tried 3 different USB cables with the same result…
Thanks,
Toby