I have multiple Wio Links set up sometime ago no problem.
Now trying to add a new Wio Node with a Grove Magnetic Switch connected to UART0/I2C0/D0
When trying to update the firmware either through the iOS app or via the API I get the same error displayed:
</s>sh: 1: make: not found<e>
Even fails if I use one of the Grove modules previously configured correctly (PIR)