Are the pictures temporarily stored on the camera eeprom before they are sent using the serial connection? Or do I need to store the on a sd card for example?
How many Mb is a average picture (JPEG)? Just to get a idea
I want to use the camera for a wireless project using the nrf24L01 but I don’t know if the wireless transfer rate is fast enough when a lot of images are sent?
Are the pictures temporarily stored on the camera eeprom before they are sent using the serial connection? Or do I need to store the on a sd card for example?
You may choose to download the pic from EEProm or ask the module to send via serial directly.
How many Mb is a average picture (JPEG)? Just to get a idea
About 15-25KB in size.
We haven’t use this module in practical project yet, maybe you could refer to the great walkthough: kalarakis.gr/Entry_001138.doc
Thanks for the reply Still a few question remaining:
I want to send the still pictures or video wireless to a host. Sending pictures wireless is not a problem.
This is a single file that I will store on a SD card and send wireless to the host.
What format is the video (i am not experienced on this area)? Will this be separate pictures send with a high rate (frame rate)? Or is this a raw format (one stream)? I ask this question because I also want to send video using wireless if possible. I’ve heard that sending a raw format (one continuous file) is very difficult for a beginner.
How fast can pictures be taken using the still mode?
You may refer to the manual: seeedstudio.com/depot/datash … 0UM_V4.pdf
It outputs JPG, the capture speed varies according to the resolution. Plz let me know if other question