Tutorial: Reading Water Flow rate with Water Flow Sensor

Is the amplitude voltage level of pulse signal dependent on the input voltage level? For example if the input voltage is 24 V then will the amplitude level of the pulse be 24 V ?