Hello everyone,
I’m trying to use the Seeed XIAO nRF52840 v1.0 board to connect via bluetooth/BLE to the nRF Connect app on my iPhone 12 Pro Max.
I’m on MacBook Pro (16-inch, 2021) with M1 Pro chip running macOS Monterey version 12.1 running Arduino 1.8.19 with the ArduinoBLE library version 1.3.2 installed.
I have connected my seeed to my MacBook Pro with a USB-C data AND power cable(learned that some cables only have power), and also uploaded the Blink example program to the seeed to verify that I could actually program the seeed.
I tried following this:
Send/Receive Data to Mobile App with XIAO BLE nRF52840 Sense
How to use nRF Connect App with Seeed XIAO BLE nRF52840 Sense
example, but I get these errors:
WARNING: library ArduinoBLE claims to run on samd, megaavr, mbed, apollo3, mbed_nano, mbed_portenta, mbed_nicla, esp32 architecture(s) and may be incompatible with your current board which runs on nrf52 architecture(s).
/Users/matthew/Documents/Arduino/libraries/ArduinoBLE/src/utility/HCIUartTransport.cpp:33:2: error: #error “Unsupported board selected!”
33 | #error “Unsupported board selected!”
| ^~~~~
/Users/matthew/Documents/Arduino/libraries/ArduinoBLE/src/utility/HCIUartTransport.cpp:99:40: error: ‘SerialHCI’ was not declared in this scope; did you mean ‘Serial’?
99 | HCIUartTransportClass HCIUartTransport(SerialHCI, 912600);
| ^~~~~~~~~
| Serial
exit status 1
Error compiling for board Seeed XIAO nRF52840 Sense.
I found the HCIUartTransport.cpp file and changing ‘SerialHCI’ to ‘Serial’, but that caused a number of other errors, making me think that that was not the root of the problem.
Does anyone understand the problem or have any suggestions of things to try? I would be very grateful for any guidance you can provide.
Thank you, Matthew