关于“Wio Terminal”分类

I still had no change in the LCD.

/*
Test the tft.print() viz embedded tft.write() function

This sketch used font 2, 4, 7

Make sure all the display driver and pin comnenctions are correct by
editting the User_Setup.h file in the TFT_eSPI library folder.

#########################################################################
###### DON'T FORGET TO UPDATE THE User_Setup.h FILE IN THE LIBRARY ######
#########################################################################

*/

This is the part that is confusing. Am I supposed to change something ? if so, what and where ??
Because this is preloaded in the image, it makes me think there is nothing to change.