Let me share the options I have in mind to deal with this:
Option a: hiring a dev to create the libraries the “To do” sensors needed
Option b: getting an Arduino Uno (slave) with grove hat and with python do a serial communication with a rpi board (master)? this is a bit too much but may work?
Option c: I guess simply installing Arduino IDE on rpi will not make the non-compatible Grove sensors compatible?
thanks for this guy did a USB comm protocol Raspberry Pi to Arduino Serial USB Communication - YouTube more interesting, however, I am in touch with the Grove dev and I hope to convince him or hire him since I prefer using the 8-hub i2p in rpi among other devices without arduino