The nRF52840 can wake up from DeepSleep using GPIO as a signal source, but the following settings alone often cause the device to wake up without a signal.
nrf_gpio_cfg_sense_input(PIN_WAKEUP, NRF_GPIO_PIN_PULLUP, NRF_GPIO_PIN_SENSE_LOW);
NRF_POWER->SYSTEMOFF = 1;
The prevention method is described in “6.10.2 PORT event” of the datasheet, and following this method will avoid unintended wakeups. See also 6.10.4.5 EVENTS_PORT, 6.10.4.6 INTENSET, 6.10.4.7 INTENCLR.
NRF_GPIOTE->INTENCLR |= 0x80000000; // disable interrupt
nrf_gpio_cfg_sense_input(PIN_WAKEUP, NRF_GPIO_PIN_PULLUP, NRF_GPIO_PIN_SENSE_LOW); // configure gpio
NRF_GPIOTE->EVENTS_PORT = 0; // Event not generated
NRF_GPIOTE->INTENSET |= 0x80000000; // enable interrupt
NRF_POWER->SYSTEMOFF = 1; // enter to DeepSleep
I hope this will be helpful to those interested.
For reference, here is the sketch I used for the experiment.
//----------------------------------------------------------------------------------------------
// BSP : Seeed nRF52 Borads 1.1.8
// Board : Seeed nRF52 Borads / Seeed XIAO nRF52840 Sense
//----------------------------------------------------------------------------------------------
// See datasheet "6.10.2 Port event"
// In order to prevent spurious interrupts from the PORT event while configuring the sources, the user
// shall first disable interrupts on the PORT event (through INTENCLR.PORT), then configure the sources
// (PIN_CNF[n].SENSE), clear any potential event that could have occurred during configuration
// (write '0' to EVENTS_PORT), and finally enable interrupts (through INTENSET.PORT).
// 2025/01/21
#include <Adafruit_SPIFlash.h> // 5.0.0, NOTE:need to deleted /Documents/Arduino/libraries/SdFat
#include <flash_devices.h>
// for flashTransport definition
Adafruit_FlashTransport_QSPI flashTransport;
Adafruit_SPIFlash flash(&flashTransport);
static const SPIFlash_Device_t my_flash_devices[] = {P25Q16H,};
const int flashDevices = 1;
#define PIN_WAKEUP (28) // D0:(2), D1:(3), D2:(28), D3:(29), D4:(4), D5(5), D6(43), D7(44), D8(45), D9(46), D10(47)
void setup()
{
// Enable DC-DC converter Mode
NRF_POWER->DCDCEN = 1; // Enable DC/DC converter for REG1 stage
// on board Flash enter to Deep Power-Down Mode
flash.begin(my_flash_devices, flashDevices);
flashTransport.begin();
flashTransport.runCommand(0xB9); // enter deep power-down mode
delayMicroseconds(5); // tDP=3uS
flashTransport.end();
// LED on for 1 sec.
digitalWrite(LED_GREEN, LOW);
delay(1000);
digitalWrite(LED_GREEN, HIGH);
// https://forum.seeedstudio.com/t/xiao-ble-long-boot-up-time/280116/13
// NRF_POWER->GPREGRET = 0x6D; // Option : Set GPREGRET0 to 0x6D (DFU SKIP)
NRF_GPIOTE->INTENCLR |= 0x80000000; // disable interrupt for event PORT
// nrf_gpio_cfg_sense_input(PIN_WAKEUP, NRF_GPIO_PIN_PULLDOWN, NRF_GPIO_PIN_SENSE_HIGH); // configure gpio for wakeup event
nrf_gpio_cfg_sense_input(PIN_WAKEUP, NRF_GPIO_PIN_PULLUP, NRF_GPIO_PIN_SENSE_LOW); // configure gpio for wakeup event
NRF_GPIOTE->EVENTS_PORT = 0; // Event not generated
NRF_GPIOTE->INTENSET |= 0x80000000; // enable interrupt for event PORT
// enter to Deep Sleep Mode
NRF_POWER->SYSTEMOFF = 1;
}
void loop()
{
}
Whether this was your objective or not, this is the best post on how to practically setup deep sleep with the XIAO that I know of. Thank you