I have several Lora E5 Minis. They work fine when trying to connect to the Lora Gateway every 10 seconds (it is the default period of time for this device when I program it using STM 32 CubeIDE). I want to extend this period to 1 minute. How do I do it using the STM 32 CubeIDE? Can I find it inside the IOC file?
Look for a HAL_Delay() or a similar function that specifies the delay between transmissions.
If you find HAL_Delay(10000); (10 seconds in milliseconds), change it to HAL_Delay(60000); (1 minute in milliseconds).
I found it alone but have not tested it yet because my infrastructure isn’t in my town or home, and I will be there after a few days.
Thank you for being so supportive,
I will answer when I am there, and I hope it will work as expected.
@liaifat85 it works nice ![]()
@marekpow
How did you set it to 1 minute?
Is it related to the APP_TX_DUTYCYCLE define?
I’d appreciate your answer.
Look for a HAL_Delay() or a similar function that specifies the delay between transmissions.
If you find HAL_Delay(10000); (10 seconds in milliseconds), change it to HAL_Delay(60000); (1 minute in milliseconds)