Hi…
I am trying to run this wonderful shield in a arduino mega 2560…
My problem is with the clock, only shows 45:-05 (points are blinking normal) and temperatures seems to work fine.
Load the RealTimeClock example in arduino 1.0.5.
Board is Arduino Mega 2560 or Mega ADK
I can compile and upload perfectly.
I can enter in menu pressing (very fast) K3… When I press UP to hours, It shows numbers higher than 24 and press DOWN, shows real hours numbers.
When I finish the setup, return to clock 45:-05.
Is there a special config to using with mega?
Thanks a lot!
Rafael