Third-party Firmware for DSO Nano

The latest version I’ve seen of the “Paul” firmware is V1.4, and it’s available here:

download/file.php?id=147

Administrators, could we have a pinned thread with links to the most recent firmware releases available, both the Seeed versions and the third-party versions, and the source files?

If someone new didn’t happen to notice that V1.4 of the Paul firmware was buried in some thread somewhere, they might be very disappointed with the performance of the DSO Nano. I’m using V1.4 on a daily basis, and it is the most stable, most usable, and best looking of the various firmwares I have tried. The use of the “M” button to change the function of the cursor keypad rather than wasting either up/down or right/left for menu navigation is the main thing which makes the DSO Nano a real, usable tool. The pop-up screen which shows all computed measurements at once is great, and makes a huge difference when actually trying to analyze a signal.

Where did the “Paul” firmware come from? Is “Paul” continuing development on his branch? Does he accept donations?