Thermal imaging camera with better MLX90640 grove sensor

Below is the sketch, I was using the two libraries I downloaded as well.

It reaches out to the device, but nothing happens after that first message is sent

It outputs Failed to load system parameters.

Blockquote
/*
Output the temperature readings to all pixels to be read by a Processing visualizer
*/

#include <Wire.h>

#include “MLX90641_API.h”
#include “MLX90641_I2C_Driver.h”

#define debug SerialUSB

const byte MLX90641_address = 0x33; //Default 7-bit unshifted address of the MLX90641
#define TA_SHIFT 8 //Default shift for MLX90641 in open air

uint16_t eeMLX90641[832];
float MLX90641To[192];
uint16_t MLX90641Frame[242];
paramsMLX90641 MLX90641;
int errorno = 0;
void setup() {
Wire.begin();
Wire.setClock(400000); //Increase I2C clock speed to 400kHz

debug.begin(115200); //Fast debug as possible

while (!debug); //Wait for user to open terminal
debug.println("MLX90641 IR Array Example");

if (isConnected() == false) {
    debug.println("MLX90641 not detected at default I2C address. Please check wiring. Freezing.");
    while (1);
}

//Get device parameters - We only have to do this once
int status;
status = MLX90641_DumpEE(MLX90641_address, eeMLX90641);
errorno = status;//MLX90641_CheckEEPROMValid(eeMLX90641);//eeMLX90641[10] & 0x0040;//

if (status != 0) {
    debug.println("Failed to load system parameters");
   while(1);
}

status = MLX90641_ExtractParameters(eeMLX90641, &MLX90641);
//errorno = status;
if (status != 0) {
    debug.println("Parameter extraction failed");
   // while(1);
}

//Once params are extracted, we can release eeMLX90641 array

//MLX90641_SetRefreshRate(MLX90641_address, 0x02); //Set rate to 2Hz
MLX90641_SetRefreshRate(MLX90641_address, 0x03); //Set rate to 4Hz
//MLX90641_SetRefreshRate(MLX90641_address, 0x07); //Set rate to 64Hz

}

void loop() {
long startTime = millis();
float vdd = 0;
float Ta = 0;

for (byte x = 0 ; x < 2 ; x++) {
    int status = MLX90641_GetFrameData(MLX90641_address, MLX90641Frame);

    float vdd = MLX90641_GetVdd(MLX90641Frame, &MLX90641);
    float Ta = MLX90641_GetTa(MLX90641Frame, &MLX90641);

    float tr = Ta - TA_SHIFT; //Reflected temperature based on the sensor ambient temperature
    float emissivity = 0.95;

    MLX90641_CalculateTo(MLX90641Frame, &MLX90641, emissivity, tr, MLX90641To);
}
long stopTime = millis();

debug.print("vdd=");
debug.print(vdd,2);
debug.print(",Ta=");
debug.print(Ta,2);

debug.print(",errorno=");
debug.print(errorno,DEC);


for (int x = 0 ; x < 64 ; x++) {
    debug.print(MLX90641Frame[x], HEX);
    debug.print(",");
}

delay(1000);

for (int x = 0 ; x < 192 ; x++) {
    debug.print(MLX90641To[x], 2);
    debug.print(",");
}
debug.println("");

}

//Returns true if the MLX90641 is detected on the I2C bus
boolean isConnected() {
Wire.beginTransmission((uint8_t)MLX90641_address);
if (Wire.endTransmission() != 0) {
return (false); //Sensor did not ACK
}
return (true);
}

Blockquote