When manually adding an application via a standard gateway, to The Things Network, by default TTN wishes to issue the APP EUI.
The SenseAPP Sensor documentation suggests a default APP EUI of “8000000000000004” and the HTTP GET request to sensecap.seeed.cc returns “8000000000000008” for APP EUI. When I add the latter, via TTN applications settings page, should I remove TTN assigned value for APP EUI or keep both “8000000000000008” + TTN issued value?