Hello,
Could you please check if the example code mentioned in seeedstudio.com/wiki/2.8’’_T … hield_V1.0 . It looks like the necessary pin re-mapping for Leonardo is mentioned in that code :
#elif defined(__AVR_ATmega32U4__) // leonardo
#define YP A2 // must be an analog pin, use "An" notation!
#define XM A1 // must be an analog pin, use "An" notation!
#define YM 18 // can be a digital pin, this is A0
#define XP 21 // can be a digital pin, this is A3
Thanks