Using an Arduino Uno, is it possible to use both the Motor Shield V2.0
and the 2.8 TFTouch Shield
together in the same project?
It looks like they both need digital pins 8-13. So, can they share these pins and just stack on top of each other?
Or is it impossible to use the TFT shield to interface controls with an Arduino Uno?
Would it be possible with an Arduino Mega if it won’t work with the Uno?