I just went out and bought another card - a Kingston 2G. It now runs the fat16info sketch - see below, but still having problems with the benchmark program. I’ll have a bit of a play with the other example programs now to try to get it going.
type any character to startinit time: 2
Manufacturer ID: 2
OEM ID: TM
Product: SA02G
Version: 0.4
Serial number: 1493315740
Manufacturing date: 3/2010
Card Size(blocks): 3842048
Partition Table:
part,boot,type,start,size
1,0,6,137,3841911
2,0,0,0,0
3,0,0,0,0
4,0,0,0,0
FAT Volume info for partition: 1
Volume is FAT16
clusterSize: 64
clusterCount: 60022
fatCount: 2
fatSize: 235
totalBlocks: 3841911
Root Directory:
name ext att size
Done