I have problem with my original (Kickstarter) module with inserted SIM card. Module is not running program, after powering on it restarts to USB mode. Without SIM module runs fine (i can upload sketch, have serial communication).
SIM is OK, no PIN, it works fine in newer module (bought later).
Is there anything to test? What can I try?
I tried to re-flash firmware (one from Arduino IDE) and module behaves in the same way even without any program loaded in.
Yesterday evening I spent playing with it and re-flashed the Arduino firmware. Than i was able to start with sim and it was telling just without SIM. Today it is just ok. surprise…
The module behaved in the way i was not able to keep it turned on (with two serial ports). It immediately went to flash firmware mode.