(TECH) Moving the microphone

I need more help than just the pinouts (including attachment with screenshot with this post).

According to the legend in the diagram there’s “Xadow Audio/Speaker & Microphone” and “External Devices/Headphone & Microphone”).

Assuming “Xadow Audio”, using the color coding on the diagram the labels are:

C2: SPK_OUTP (I’m assuming order isn’t important, although I’ll switch between to check)
D2: SPK_OUTN

Now according to the color coding, there are FOUR pins in the indicatedcolor:

A3: AU_VIN0_N
D3: MICBIA50
D6: GPIO4646 (1.8V)
E4: AU_VIN0_P

Two questions from here:

  1. What microphones can I use? I was thinking something like: sparkfun.com/products/9964
  2. OR could I somehow rig up a headphone/microphone jack similar to what most cell phones have?

Charlie in Houston