Dear All,
I am powering module only using PIN 3+6. Module works only, when powered 4.1-4.2V, otherwise the module sometimes restarts. What are the power consideration when powering without battery, e.g. capacitors, etc.?
Thank you
Jan
Dear All,
I am powering module only using PIN 3+6. Module works only, when powered 4.1-4.2V, otherwise the module sometimes restarts. What are the power consideration when powering without battery, e.g. capacitors, etc.?
Thank you
Jan
May be this two topics can help you!
http://www.seeedstudio.com/forum/viewtopic.php?f=71&t=6505
http://www.seeedstudio.com/forum/viewtopic.php?f=71&t=6527
Thank you for the reply.
Even with the battery connected, i still have problems when there is voltage on battery below 4.1V. I’d like to have this module in kiosk to do a call on a button, but it seems to me, taht this is not possible, with RePhone module…
The behavior is little erratic 
It just restart when you make a call?? or it restart when there is no SIM?