System_ON_Sleep of XIAO BLE

Some more observations:
Case 1:
Central => my sketch above without MSD filter
Peripheral => adafruit beacon example
Sniffer: peripheral sent out quite a lot of scan responses to central
Central serial: captured a lot less scan responses compared to above

Case 2:
Central => my sketch above with MSD filter
Peripheral => my sketch above but advertising data was reduced to a flag only

void startAdv(void)
{
// Set Flag for discovery mode, optional
Bluefruit.Advertising.addFlags(BLE_GAP_ADV_FLAGS_LE_ONLY_LIMITED_DISC_MODE);

// Construction of data packet to be advertising
if (counter == 0xFF)
{counter = 0;}
else
{counter = counter + 1;}
user_data[0] = 0x59; // little endian format for first and second entry
user_data[1] = 0x00; // (00-59) means Nordic Semi
user_data[2] = counter; // third entry increments with each advertising cycle
Bluefruit.Advertising.addData(BLE_GAP_AD_TYPE_MANUFACTURER_SPECIFIC_DATA, user_data, sizeof(user_data)/sizeof(user_data[0]));
Bluefruit.Advertising.clearData();

// Construction of scan response
scan_rsp_data[0] = 0x59; // little endian format for first and second entry
scan_rsp_data[1] = 0x00; // (00-59) means Nordic Semi
scan_rsp_data[2] = 0xD1;
scan_rsp_data[3] = 0xD2;
scan_rsp_data[4] = 0xD3;
scan_rsp_data[5] = 0xD4;
Bluefruit.ScanResponse.addData(BLE_GAP_AD_TYPE_MANUFACTURER_SPECIFIC_DATA, scan_rsp_data, sizeof(scan_rsp_data)/sizeof(scan_rsp_data[0]));

Bluefruit.Advertising.setType(BLE_GAP_ADV_TYPE_NONCONNECTABLE_SCANNABLE_UNDIRECTED);
//Bluefruit.Advertising.setType(BLE_GAP_ADV_TYPE_CONNECTABLE_SCANNABLE_UNDIRECTED);
Bluefruit.Advertising.restartOnDisconnect(true);
Bluefruit.Advertising.setIntervalMS(100, 100); // in unit of ms
Bluefruit.Advertising.setFastTimeout(5); // number of seconds in fast mode
Bluefruit.Advertising.start(5); // stop advertising after 5 seconds
}

Central serial: captured a lot of scan responses

I am wondering if central is not fast enough to catch and decode both the advertising and scan response packets in a short time. I will try to adjust the 2 payload sizes or to increase the serial buffer next time. I have spent too much time on this and my wife is not happy.