System_ON_Sleep of XIAO BLE

Based on hobbya’s suggestion, I measured the current when the peripheral only advertises.

  1. Average current for data transmission every 10 seconds
    The method the peripheral only advertise could reduce the current to 115uA, which would be a great benefit for data transmission. This can be very effective for transmitting a small amount of data.
  2. Sleep period current
    The average current during the sleep period is less than 5 uA, which is comparable to the DeepSleep mode.