this is a following up of the previous post…
xbee drivers are installed, it shows up in device manager as USB serial port (COM5), the skecth compile fine, no errors since i’ve found i had to change a couples of things in the code, but, when i hit upload button, after compiling arduino halt and the error says:
"avrdude: stk500_getsync():not in sync: resp=0x00"
x-ctu cannot read information from xbee as proposed in this page: http://www.seeedstudio.com/wiki/Zigbee_Networking_with_XBee_Series_2_and_Seeed%27s_Products#Using_Digi.27s_X-CTU_.28XCTU.29_Software
i am using arduino 1.0.4
grove - xbee carrier
windows 7 64 bits
bluetooth standalone
any help would be wonderful