Sten carrier, solar kit and two RFBees

Hi,

I want to create a base station with one RFBee attached to an Arduino and a remote node that uses and RFBee with the Stem carrier.

How do I need to program these to do this? Which board should I select to program them?

Till now nothing actually works.

Has anyone done this before (which seems to be very logical to do).

There is a big lack of very detailed information on the Seedstudio site and a lot of info is scattered everywhere. Such a shame because the hardware has potential.

Any suggestions?