Hi,
Please feel free to ask any questions on the forum.
Binary sketch size: 1010 bytes (of a 30720 byte maximum)
avrdude: stk500_getsync(): not in sync: resp=0x30
avrdude: stk500_disable(): protocol error, expect=0x14, resp=0x51
You can follow this step and make the right setting.
Arduino 0019 software: Tools -> Board-> Arduino Duemilanove or Nano with ATmega328 (you have set it).
Arduino 0019 software: Tools -> Board->Serial Port -> your UartSbee serial port.
OK, you can try to upload the Blink code to the stalker, and it will be fine.
How are the two switches on the UartSB supposed to be set? Mine are currently set to 5V and XBEE
You can set to 5V when the stalker works on 5V, and set to 3.3V when the stalker works on 3.3V.
The XBEE_VCC_BT switch uses to select Xbee or Bluetooth Bee when you want to use them.
Any questions?
Regards.